Packets retransmitted on connection
Description
The total number of retransmissions that have been sent to the CIP connection since it was established. Retransmissions could occur because a target is slow to respond (or is offline) or packets were lost on the wire.
Provide Feedback