Packets overwritten on connection

Description
The total number of send attempts (not including retransmissions) that were made on the CIP connection before the response to a previous request was received. This could occur because a request timed out while it was pending on a connection or because the client canceled the request.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal