Optimized Packets

Description
An optimized packet is established by FactoryTalk Linx to group multiple data item requests into a single response from a Logix controller. The
Optimized Packets
attribute is obtained from FactoryTalk Linx and provides the quantity of these grouped data requested established with the Logix controller referenced via a FactoryTalk Linx shortcut.
This attribute is available when there is a client reading or subscribing tags from a controller. It is listed under:
  • FactoryTalk Linx
    >
    DataProviders
    > ControlLogix controllers
  • FactoryTalk Linx Instance02
    >
    DataProviders
    > ControlLogix controllers
Value
  • Type
    : Number
  • Engineering unit
    : N/A
  • Default value
    : 0
  • Refresh frequency
    : Changed when a FactoryTalk client adds or removes tags subscriptions with FactoryTalk Linx
    TIP:
    When removing tags, FactoryTalk Diagnostics Counter Monitor needs about five minutes to update the value.
  • Invalid value
    : N/A
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal