Total Symbol Count
Description
It represents the number of individual tags in the controller scope and all program scope.
TIP:
If a tag is defined as a structure or array, the individual members of the structure and array elements are not included in the symbol count.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx > DataProviders >Controller> Namespace
Value
- Type: Integer
- Source: This value is generated by the FactoryTalk Linx server.
- Updates: This value is loaded when FactoryTalk Linx uploads the controller namespace.
Provide Feedback