Symbol Synchronization State

Description
FactoryTalk Linx must maintain a copy of the tags and datatypes defined in a Logix controller to optimize communications. When a connection to the controller is initiated or a significant change is made to the controller, FactoryTalk Linx must reload or synchronize all the controller’s tag and datatype definitions. This attribute indicates the current or last state of this synchronization process. It is obtained from FactoryTalk Linx.
FactoryTalk Linx must establish a connection with a controller. This attribute is listed under:
  • FactoryTalk Linx
    >
    DataProviders
    > ControlLogix controllers >
    Namespace
  • FactoryTalk Linx Instance02
    >
    DataProviders
    > ControlLogix controllers >
    Namespace
Value
  • Type
    : String
  • Engineering unit
    : N/A
  • Values
    :
    • INITIAL SYNCHRONIZATION
      FactoryTalk Linx starts to upload namespace from the controller.
    • RESYNCHRONIZE
      FactoryTalk Linx restarts to upload namespace from the controller.
    • SYNCHRONIZATION IN PROGRESS
      FactoryTalk Linx is uploading the namespace.
    • SYNCHRONIZATION COMPLETED
      FactoryTalk Linx completes the uploading of the namespace.
    • SYNCHRONIZATION FAILED
      Unable to upload the namespace.
    • ALL CONNECTIONS LOST
      The connections between FactoryTalk Linx and the controller are all closed.
    • DOWNLOAD IN PROGRESS
      Studio 5000 Logix Designer is downloading a project to the controller.
  • Refresh frequency
    : Changed when the progress state changes
  • Invalid value
    : N/A
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal