Symbol Count

Description
Represents the number of individual tags in a program scope within the controller.
TIP:
If a tag is defined as a structure or array, the individual members of the structure and array elements are not included in the symbol count.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx > DataProviders >
    Controller
    > Namespace > Programs > Program:
    ProgramName
    TIP:
    "ProgramName" will be replaced by the name of a program defined in the controller. For example, "Program:MainProgram".
Value
  • Type: Integer
  • Source: This value is generated by the FactoryTalk Linx server.
  • Updates: This value is loaded when FactoryTalk Linx uploads the controller namespace.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal