Change Detection LOW
Description
The low part of an audit value (a unique 64-bit integer) for controller change detection in
Studio 5000 Logix Designer®
. By inspecting this value, you can detect if changes
are made to Logix5000™
controllers.Provide Feedback