WritePacketsQueued

Description
Indicates the number of write packets that the Legacy data provider currently has waiting to send to the
FactoryTalk Linx
communications engine. The maximum queue depth is 512. If the combined number of poll and write requests pending exceeds 512, an error message is generated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal