MaximumPacketsPending
Description
Specifies the maximum number of combined poll and write requests that this data provider will hold outstanding to the target device before the data provider starts queuing requests. The value supplied by the data provider is network dependent, but is user adjustable. Setting this counter to a value higher than 100 may result in timeouts.
Provide Feedback