Search
FactoryTalk Diagnostics Counter Monitor
DevicePath
Description
Identifies the communication route that
FactoryTalk Linx
is using to communicate with the target controller (for example, Ethernet.192.168.100.101, SerialDF1.1, DH+.055, etc.).
Legacy Shortcut Node
Use FactoryTalk Diagnostics Counter Monitor with FactoryTalk Linx
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal