Service Status

Description
This value indicates the status of the FactoryTalk Linx Gateway RTD service.
  • RUNNING: indicates that the service is running and operational.
TIP:
The FactoryTalk Linx Gateway RTD service has multiple states, including starting, running, stopping, and stopped. However, in Diagnostics Counter Monitor, only running will be shown under the Service Status counter. If the service isn’t in the running state, this counter will not appear.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway RTD Server
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway RTD server.
  • Updates: This value is loaded when the service initially starts.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal