LicenseCount
Description
The FactoryTalk Linx Gateway RTD server obtains the activation from FactoryTalk Activation Manager. The counter indicates the maximum data item or tag capacity of the activation in use support. If no activation is found, the value is 0.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway RTD Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway RTD server.
- Updates: This value is loaded when the service initially starts.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback