Count against Activation
Description
This counter indicates the number of tags that have been added to the server. This number includes active and inactive tags. Duplicate tags count as a single tag.
TIP:
Count against Activation provides a real-time tag count rather than an accumulated value since the service started. The value will change as tags are added or removed.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway RTD Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway RTD server.
- Updates: This value increases when an RTD client adds a new tag and decreases when removing an existing tag.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback