Client Call DisconnectData
Description
This counter indicates the number of requests from RTD clients to disconnect data.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway RTD Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway RTD server.
- Updates: This value increases when an RTD client requests to disconnect data.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback