Client Call ConnectData

Description
This counter indicates the number of requests from RTD clients to connect data.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway RTD Server
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway RTD server.
  • Updates: This value increases when an RTD client requests to connect data.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal