Total Items

Description
This counter indicates the number of monitored data items in the subscription.
TIP:
Total item provides a real-time item count rather than an accumulated value since the service started. The value will change as items are added or removed.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID) > Subscription (ID)
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value increases when an OPC UA client adds a monitored data item to the subscription and decreases when removing an existing data item.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal