Subscription Id
Description
This value indicates the ID of the subscription. This ID is randomly assigned by the FactoryTalk Linx Gateway OPC UA server upon connection establishment. It serves as a unique identifier for each subscription and allows the server to distinguish between multiple subscription connections and manage communication with them. For example, 1234567890.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID) > Subscription (ID)
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when an OC UA client creates a subscription.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback