Publishing Interval

Description
This value indicates the time intervals (in milliseconds) between data updates sent by the OPC UA server to client subscriptions. It represents how frequently the server is publishing updates for the monitored data items or variables to subscribed clients.
For example, a value of 100 indicates that the OPC UA server is publishing updates for the monitored data items to client subscriptions every 100 milliseconds.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID) > Subscription (ID)
Value
  • Type: Double
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value is retrieved when the configuration changes in the OPC UA client.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal