Trusted Certificate Store
Description
This value indicates the Windows file location of the certificates trusted by the FactoryTalk Linx Gateway OPC UA server list. For example, C:\ProgramData\Rockwell\FactoryTalk Linx Gateway\PKI\trusted\.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when the service initially starts.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback