Service Start Timestamp

Description
This value indicates the precise time at which the FactoryTalk Linx Gateway service starts.
For example, ā€œ2024-01-26T01:09:45.502Zā€ represents a connection established on January 26, 2024, at 1:09:45 AM and 502 milliseconds in Coordinated Universal Time (UTC).
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value is loaded when the service initially starts.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal