Remove Subscription calls
Description
This counter indicates the number of requests from OPC UA clients to remove a subscription. It is a server-level cumulative count and reflects the requests from various OPC UA clients.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value increases when an OPC UA client removes a subscription.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback