Outgoing Public Certificate

Description
This value indicates the Windows file location where outgoing public certificates are stored on the computer running FactoryTalk Linx Gateway. These outgoing public certificates will be transmitted to OPC UA clients upon establishing a connection or session. For example, C:\ProgramData\Rockwell\FactoryTalk Linx Gateway\PKI\own\cert_ftgw_opcua_server.der.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value is loaded when the service initially starts.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal