LDS Registration URL
Description
This value indicates the URL used by the FactoryTalk Linx Gateway for registration purposes. By default, this value directs to the Local Discovery Server (LDS) installed on the same computer where FactoryTalk Linx Gateway is running. However, you can configure the URL to point to an LDS or a Global Discovery Service (GDS) running on a different computer. For example, opc.tcp://USER:4840/.
For the latest version of the OPC LDS, visit the OPC Foundation's download site https://opcfoundation.org/developer-tools/developer-kits-unified-architecture/local-discovery-server-lds/.
Find more information on OPC UA Discovery and Global Services, visit: https://opcfoundation.org/developer-tools/specifications-unified-architecture/part-12-discovery/.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when the service initially starts.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback