Count against Activation
Description
This counter indicates the number of unique tags currently in use. The number includes active and inactive tags. Duplicate tags count as a single tag.
TIP:
Count against Activation provides a real-time tag count rather than an accumulated value since the service started. The value will change as tags are added or removed. However, in cases where a client stops responding or disconnects without removing requested tag items, the count may become inaccurate. To resolve this issue, restart the FactoryTalk Linx Gateway OPC UA server.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value increases when an OPC UA client adds a new tag and decreases when removing an existing tag.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback