Client Disconnect calls
Description
This counter indicates the number of times the FactoryTalk Linx Gateway OPC UA server has received disconnection requests from OPC UA clients.
TIP:
If the FactoryTalk Linx Gateway Configuration dialog is closed, the Client Disconnect Calls count will increment.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value increases when an OPC UA client requests disconnection from the FactoryTalk Linx Gateway OPC UA server.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback