Client Connections that failed after reconnecting

Description
This counter indicates the number of unsuccessful connection attempts from OPC UA clients to the FactoryTalk Linx Gateway OPC UA server after establishing the initial connection. Failed connections can occur due to various reasons, such as network issues, authentication failures, or communication protocol errors.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value increases when an OPC UA client fails to connect to the FactoryTalk Linx Gateway OPC UA server.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal