Certificate Revocation List

Description
This counter indicates the Windows file location of all the revoked certificates from OPC clients. For example, C:\ProgramData\Rockwell\FactoryTalk Linx Gateway\PKI\crl\.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value is loaded when the service initially starts.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal