Active Secured Connections
Description
This counter indicates the number of OPC UA clients connected to the OPC UA server with the FactoryTalk Security User authentication.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value increases when an OPC UA client connects to the server with the FactoryTalk Security User authentication and decreases when the same client disconnects.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback