Activation

Description
FactoryTalk Linx Gateway OPC UA service obtains the activation from FactoryTalk Activation Manager. This value indicates the type and tag count of the FactoryTalk Linx Gateway activation that is in effect for the selected server.
Example of an Activation value: Network 500,000 (Grace Period: 6 days, 4hrs, 4mins)
  • “Network”: indicates the activation type.
  • “500,000”: indicates the maximum number of tags allowed under the current activation.
  • “Grace Period: 6 days, 4hrs, 4mins”: The grace period is a seven-day free trial of FactoryTalk Linx Gateway, during which a user has the tag subscription capability equal to the "Professional" activation. In this case, after 6 days, 4 hours, and 4 minutes, the OPC UA clients cannot connect to FactoryTalk Linx Gateway.
TIP:
  1. The activation types are: network, network station, local, and master.
  2. If no activation is found, the value will show ‘Activation not found’.
For more information on the activation type, see
FactoryTalk Linx Gateway Help
.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value is loaded when the service initially starts.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal