Last Toolkit Error Message
Description
This value indicates the description of the last error message generated by the OPC UA toolkit used by FactoryTalk Linx Gateway to communicate using the OPC UA protocol. If there is no error message, the value appears as “None”.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value changes when the toolkit detects an error.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback