Failed Writes due to Security

Description
This counter indicates the number of failed write requests from the current OPC UA client to the FactoryTalk Linx Gateway OPC UA server. This issue occurs when the FactoryTalk Linx Gateway server cannot retrieve data from FactoryTalk Live Data, because the
Tag Write Value
permission setting is set as
Deny
in the FactoryTalk Administration Console.
The FactoryTalk Diagnostics records details such as the client, group, and item name associated with the security error for troubleshooting assistance.
To resolve this issue, set the
Tag Write Value
permission as
Allow
in the FactoryTalk Administration Console. For more instructions on the configuration, see the
FactoryTalk Services Platform Help
.
Considering the following points when configuring product policies and securable actions in the FactoryTalk Administration Console:
  • Security settings are obtained from the FactoryTalk Network Directory.
  • FactoryTalk Services Platform version 2.50 (SR5) or later supports associating the project with a specific FactoryTalk Directory.
  • FactoryTalk Services Platform version 2.80 or later supports Permission Sets and the ability to configure Guest User permissions.
  • Product Policies are not tied to a specific project, and include, among others, the following policies:
    • Securing the controller.
    • Creating a new project, either through the New Controller dialog box, or through the Translator Tool utility.
    • Updating firmware.
For more information on security setting, see the
FactoryTalk Linx Gateway Help
.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value increases when an OPC UA client fails to edit the data item because of security settings.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal