Failed to Remove Subscription calls

Description
This counter indicates the number of failed calls from the current OPC UA client to remove subscriptions within the FactoryTalk Linx Gateway OPC UA server. This may occur if the client sends an unknown or invalid subscription ID.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value increases when an OPC UA client fails to remove a subscription.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal