Failed to Monitor Items
Description
This counter indicates the number of failed requests from the current OPC UA client to monitor items within the FactoryTalk Linx Gateway OPC UA server. This may occur if the item count exceeds the maximum supported by the current activation.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value increases when an OPC UA client fails to monitor an item.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback