Create Subscription calls
Description
This counter indicates the number of requests from OPC UA clients to create subscriptions.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value increases when an OPC UA client creates a subscription.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback