Connection Timeout
Description
This value indicates the timeout duration (in milliseconds) for connection attempts to the FactoryTalk Linx Gateway OPC UA server. This timeout duration determines the maximum time that the server will wait for a response from a client during the connection process.
For example, a value of 600000 indicates that the server will wait up to 600 seconds (10 minutes) for a response from a client during connection attempts. If there is no response within this timeframe, the connection attempt will be terminated due to a timeout.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when the client connects to the server.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback