Connected Security Policy
Description
This value indicates the security policy of the communication between clients and servers.
- None
- Basic128Rsa15
- Basic256
- Basic256Sha256
- Aes128Sha256RsaOaep
- Aes256Sha256RsaPss
For more information on the OPC Foundation Security Policy, visit https://profiles.opcfoundation.org/developer-tools/.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when the client connects to the server.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback