Connected Security Mode

Description
This value indicates the security mode of the communication between clients and servers.
  • None: No specific security measures are applied.
  • Sign: Communication between clients and servers will only be signed, ensuring the integrity and authenticity of messages.
  • Sign & Encrypt: Communication between clients and servers will be signed and encrypted, ensuring the integrity, authenticity, and confidentiality of messages.
  • Sign + Sign & Encrypt: Allow both above options, providing flexibility to apply appropriate security measures for specific requirements.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value is loaded when the client connects to the server.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal