Client IP Address
Description
This value indicates the IP address of the current OPC UA client connected to the FactoryTalk Linx Gateway OPC UA server. For example, 192.168.1.1.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when the client connects to the server.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback