Client Id
Description
This value indicates the ID of the OPC UA client. This ID is randomly assigned by the FactoryTalk Linx Gateway OPC UA server upon connection establishment. It serves as a unique identifier for each OPC UA client and allows the server to distinguish between multiple client connections and manage communication with them.
Example of a client ID: ns=2; i=4171769704
- “ns=2” indicates that the namespace index is 2.
- “i=4171769704” indicates that the numeric identifier value is 4171769704.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when the client connects to the server.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback