Authentication
Description
This counter indicates the method used to authenticate users when connecting to the FactoryTalk Linx Gateway OPC UA server. There are two methods:
- Anonymous: The value displays as “Anonymous”, indicating that the connection is made without user authentication.
- FactoryTalk Security User: The value displays the username of the authenticated FactoryTalk Security user.
TIP:
You can configure the settings for FactoryTalk Security users in the FactoryTalk Administration Console.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server > Client (ID)
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value is loaded when the client connects to the server.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback