Service Status
Description
This counter indicates the status of the
FactoryTalk Linx Gateway
OPC DA service:- Starting: indicates that the service is in the process of starting up.
- Running: indicates that the service is running and operational.
- Stopping: indicates that the service is in the process of shutting down.
- Stopped: indicates that the service has stopped and is not operational.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value is loaded when the service initially starts.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback