Failed Writes
Description
This counter indicates the number of times when the write requests from OPC DA clients are unsuccessful. It is a server-level cumulative count and reflects the failures from various OPC DA clients.
The FactoryTalk Diagnostics will show the client, group, and item name that failed.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value increases when an OPC DA client fails to edit the data item.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback