Failed to Add Items
Description
This counter indicates the number of items that the OPC DA clients are unable to add. It is a server-level cumulative count and reflects the failures from various OPC DA clients.
The FactoryTalk Diagnostics Event Log will show the items that are unable to be added. The event log messages may originate from either "FactoryTalk Linx Gateway" or "FactoryTalk Service."
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value increases when an OPC DA client fails to add an item.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback