Count against Activation

Description
This counter indicates the number of unique tags currently in use. The number includes active and inactive tags. Duplicate tags count as a single tag.
TIP:
Count against Activation provides a real-time tag count rather than an accumulated value since the service started. The value will change as tags are added or removed. However, in cases where a client stops responding or disconnects without removing requested tag items, the count may become inaccurate. To resolve this issue, restart the FactoryTalk Linx Gateway OPC DA server.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value increases when an OPC DA client adds a new tag and decreases when removing an existing tag.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal