Callbacks to Process
Description
The number of callbacks in the queue from
FactoryTalk Linx Gateway
to the client. Ideally, the value of this counter is 0 (zero), but there may be some fluctuation. If the value continues to increase, it indicates the client has fallen behind and is too slow. Increase the scan rate (for example, from 250 ms to 1000 ms).Provide Feedback