Add Item calls

Description
This counter indicates the number of requests from all OPC DA clients to add items. It is a server-level cumulative count and reflects the requests from various OPC DA clients.
TIP:
An OPC DA client can add multiple items using a single Add Item call.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value increases when an OPC DA client requests to add an item.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal