Add Group calls
Description
This counter indicates the number of requests from all OPC DA clients to add groups. It is a server-level cumulative count and reflects the requests from various OPC DA clients.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value increases when an OPC DA client requests to add a group.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback