Activation
Description
This is a string that contains the FactoryTalk Linx Gateway activation type and tag count that is in effect for the selected provider; for example, Network 5000.
TIP:
For more information about activation type, see FactoryTalk Linx Gateway Online Help.
Provide Feedback