UpdateRate
Description
This counter indicates the frequency of updates of the OPC DA group.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_X> GroupX
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value is retrieved when the configuration changes in the OPC DA client.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback