State

Description
The counter indicates the state of the OPC DA group. Valid states include:
  • Active: indicates that the OPC DA group is operational and processing data.
  • Inactive: indicates that the OPC DA group is not operational and is not processing data.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_
    X
    > Group
    X
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value is retrieved when the configuration changes in the OPC DA client.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal